Create Page Elements

Page Elements are the building blocks of a Page Template. You could start the process by building some Page Templates, but you might appreciate having your Elements ready first. Thus, this set of topics discusses each Element type. The next set of topics discusses putting them all together in a Page Template.


Prerequisite

To configure any Page Element, you need a blank page to work on. It is merely a canvas for you as you work with your elements.

To get a blank page:

  1. In Designer XI, click the Layout tab at the top of the interface.

  2. Click the Add Element tool.

  3. In the Add Element dialog, click Blank Page.

  4. Choose a page size. While creating Page Elements, pick a typical page size. That way you know the bounds of a final print while creating the Elements.

  5. At the bottom of the Add Element dialog, click Add.

  6. You now have a canvas to work on as you configure your Page Elements.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?