Checklist for a New Component Type
Designer XI supports the most common Component Types for electric and gas networks, and the application continues to grow and add support for more components. But when a new component is introduced, how do you incorporate it into your existing implementation? Use this checklist to guide you through the process of supporting a new component type:
-
Identify the features in your GIS that will be represented by the component type. These features most likely already exist. Using Generic Line Components (GLCs) as an example, you would make a short list of the features you want to map to the GLCs, such as telecommunication lines, pipe casings, bond wires, or other non-networked line features you want to reference in your designs.
-
Ensure the features you identified in Step 1 are in your company’s asset map, and Re-Publish the Network Feature Service.
-
Update the Schema using the Schema Editor in Solution Center to map the features and their fields to the component type.
-
Configure the Equipment Specifications (specs) and update your rules for Dynamic Spec Assignment.
-
Create compatible units (CUs), Macro CUs, and Non-Drawn CUs to support the new component type optionally creating CU Categories if desired.to support the new component type.
-
Update your Design Style to show the new component type for all required work functions (install, remove, etc.).
-
In the client application, create a “sandbox” or “throwaway” design and test the new component type.