Recognized Types for Design Style Symbols

The table below includes the component types that can be used within the arcade script. For example, if you were working with transformers within the arcade script, you would utilize “xfr” as the syntax within the script. That is how the application knows you are scripting transformers. In the previous topic, we recommended incorporating the types as part of the symbol Keys. This makes it easier to match Key to type when working within the arcade script. This makes more sense when you view the arcade script, so remember you can download a sample at Designer XI Samples to view a finished script.

Type

Meaning 

att 

PoleAssembly 

brkr     

Breaker 

cap      

Capacitor 

capb     

CapacitorBank 

cnd      

ConduitSystem 

cond 

Conductor 

condb 

ConductorBank 

cutpoint   

CutPoint 

der      

DistributedEnergyResource 

ev       

ElectricVehicleCharger 

fib      

FaultIndicatorBank 

fitting 

Fitting 

fuse     

Fuse 

fuseb    

FuseBank 

gen      

Generator 

genb     

GeneratorBank 

ggpc 

GasGenericPointComponent 

glc

GenericLineComponent

guide 

ElectricLayoutGuide 

guide 

GasLayoutGuide 

guy      

Guy 

jmp 

Switch 

loadbreak 

Switch 

misc 

SwitchBank 

mtrset 

MeterSetting 

ncb      

ElectricNetworkComponentBank 

networkcomponent         

ElectricNetworkComponentBank 

node     

ConnectivityNode 

oh_pcil 

OhPathComponentInsertionLocation 

opg      

OffsetPathGuide 

pipe 

Pipe 

poi 

ElectricLayoutPointOfInterest 

poi 

GasLayoutPointOfInterest 

pole 

Pole 

riser 

Riser 

sb 

SectionalizerBank 

sec 

Sectionalizer 

sp  

ServicePoint 

spanguy 

SpanGuy 

src      

FeederSource 

srcb     

FeederSourceBank 

struct 

SurfaceStructure 

swb 

SwitchBank 

swb 

SwitchBank 

switch 

Switch 

trnch    

ConduitSystem 

ug_pcil 

UgPathComponentInsertionLocation 

valve 

Valve 

vr 

VoltageRegulator 

vrb 

VoltageRegulatorBank 

wl 

WorkLocation 

xfr 

Transformer 

xfrb 

TransformerBank 

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.