ArcGIS Server with Portal for ArcGIS Federation

Federating an ArcGIS Server site with Portal for ArcGIS integrates the security and sharing models of your Portal with one or more ArcGIS Server sites.

IMPORTANT: Refer to Esri’s Federate a server site article to federate your server site. It is crucial to remember that while Esri supports Integrated Windows Authentication (IWA), Schneider Electric doesn’t. Do not follow the guidance regarding IWA in the linked article.

After you finish federating your server site with Portal for ArcGIS, you need to consider communication protocols and security. By default, both ArcGIS Server and Portal for ArcGIS allow for HTTP and HTTPS communication. Schneider Electric supports only HTTPS communication. Thus, continue onto the next topic (Change ArcGIS Server Communication Protocol) to configure HTTPS communication.

Change ArcGIS Server Communication Protocol

Follow these steps to change the ArcGIS Server communication protocol, if needed:
  1. Open the ArcGIS Server Administrator Directory and log in as a user who has administrative permissions. The Administrator Directory URL is formatted as such: https://gisserver.domain.com:6443/arcgis/admin.
  2. Click Security > Config > Update.
  3. For Security Configuration > Protocol, choose HTTPS Only.
  4. Click Update to restart your ArcGIS Server site.
  5. Wait for the server to restart completely before proceeding.
  6. Log out of the Administrator Directory.

NOTE: It takes ArcGIS Web Adaptor approximately one minute to recognize changes to your site’s communication protocol.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?