Recognized Label Fields for Design Styles

The tables below show what to type in the Text String field when creating a Design Style label. For example:

These tables include all the recognized fields that can be used for labeling.

General

Type of Component

Text String for the Label

All Components

[Type]

[SpecType]

[WorkFunction]

All Components with a Facility ID

[Name]

Conduit

[ConduitType]

Components with Measured Length

[MapLength]

[MeasuredLength]

Point Component Rotation

[Angle]

Work Locations

[Number]

Electric

Type of Component

Text String for the Label

Conductor

[Material]

[Feeder]

[ConductorType]

Energized Component

[VoltageClass]

[Energized]

[PhaseCount]

Switch

[OpenPhases]

Transformer

[RatedkVA]

Gas

Type of Component

Text String for the Label

Fitting

[Diameter]

[Material]

[LocalizedMaterial]

Pipe

[Diameter]

[Material]

[LocalizedMaterial]

Valve

[Diameter]

[Material]

[NormalPosition]

[LocalizedMaterial]

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.