Hosted Services

Both Design Storage Service and Edge Service can now be implemented as hosted by Schneider Electric or installed on-premises. The benefits of using these hosted service are the same as other Schneider Electric hosted services.

  • Hosted services allow lower total cost of ownership for the customer because Schneider Electric deploys, manages, troubleshoots, and upgrades these services on behalf of the customer.

  • There is no need to allocate hardware, maintain OS security patches, install the service, or update the service.

  • Customers don’t need to manage the IT security for an IIS service that needs to be able to communicate with external systems.

  • You are always ensured to have the latest version of the service.

  • Hosted services support multi-tenant environments.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.