1PH4W Multi LN updates (iEM3155 / iEM3255 / iEM3355)
Addition of each phase reactive energy import register
|
Address |
Register |
Action |
Size |
Type |
Units |
Description |
|---|---|---|---|---|---|---|
|
0xB047 |
45128 |
R |
2 |
Float32 |
kVARh |
Reactive Energy Delivered Phase A |
|
0xB049 |
45130 |
R |
2 |
Float32 |
kVARh |
Reactive Energy Delivered Phase B |
|
0xB04B |
45132 |
R |
2 |
Float32 |
kVARh |
Reactive Energy Delivered Phase C |
You can access each phase reactive energy import values using INT64 or Float 32 register format.
Addition of each phase name register
|
Address |
Register |
Action |
Size |
Type |
Units |
Description |
Default value |
|---|---|---|---|---|---|---|---|
|
0xDEA7 |
57000 |
R |
5 |
UTF8 |
— |
Phase 1 Name |
PH1 Eng Impt |
|
0xDEAC |
57005 |
R |
5 |
UTF8 |
— |
Phase 2 Name |
PH2 Eng Impt |
|
0xDEB1 |
57010 |
R |
5 |
UTF8 |
— |
Phase 3 Name |
PH3 Eng Impt |
Addition of one command to set the each phase name
|
Command Number |
Action |
Size |
Type |
Units |
Range |
Description |
|---|---|---|---|---|---|---|
|
6018 |
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
W |
5 |
UTF8 |
— |
String size ≤ 10 |
Phase 1 name Label |
|
|
W |
5 |
UTF8 |
— |
String size ≤ 10 |
Phase 2 name Label |
|
|
W |
5 |
UTF8 |
— |
String size ≤ 10 |
Phase 3 name Label |