DOCA0005EN-15

Primary VIF used by the meter

NOTE: E denotes the extension bit; x in the hex value is determined by bits 7 – 4 of the VIF.

Primary VIF

bin

hex

Description

Energy

E000 0011

x3

Wh with a resolution of 100 in int64

kWh with a resolution of 103 in float32

Power

E000 1110

xE

kW with a resolution of 103

Time point

E110 1101

xD

Date and time in data type F, as detailed in the M-Bus protocol documentation

Bus address

E111 1010

xA

Data type C (unsigned integer), as detailed in the M-Bus protocol documentation

Primary VIFE

1111 1101

FD

Indicates that the first VIFE is a primary VIF extension

Manufacturer-specific VIFE

1111 1111

FF

Indicates that the next VIFE is manufacturer specific

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?