DOCA0005EN-15

LonWorks communications

Characteristic

Value

Meters

Number of ports

1

iEM3175 / iEM3275 / iEM3375

Isolation

3.75 kV rms

Wire

2.5 mm2/ 14 AWG shielded twisted pair

Wire strip length

7 mm / 0.28 in

Torque

0.5 Nm / 4.4 in·lb

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?