DOCA0005EN-15

Overload Alarm (iEM3155 / iEM3255 / iEM3355)

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

0xAFC8

45001

R/WC

1

Bitmap

Overload Alarm Setup:

  • 0x0000 = Disabled
  • 0x0100 = Enabled

0xAFC9

45002

R/WC

2

Float32

kW

Pickup Setpoint

0xAFCB

45004

R/WC

1

Bitmap

Digital Output to Associate:

  • 0x0000 = Digital Output unassociated to overload alarm
  • 0x0100 = Digital Output associated to overload alarm

0xAFCC

45005

R

1

Bitmap

Activated Status:

  • 0x0000 = Alarm is inactive
  • 0x0100 = Alarm is active

0xAFCD

45006

R

1

Bitmap

Unacknowledged Status:

  • 0x0000 = Historic alarm is acknowledged by the user
  • 0x0100 = Historic alarm is unacknowledged by the user

0xAFCE

45007

R

4

DATETIME

Last Alarm - Time Stamp

0xAFD2

45011

R

2

Float32

kW

Last Alarm - Value

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?