DOCA0005EN-15

Considerations for iEM3100 series and iEM3300 series devices associated with a contactor

Connection requirements for iEM3100 / iEM3110 / iEM3115 / iEM3135 / iEM3150 / iEM3155 / iEM3165 / iEM3175 / iEM3310 / iEM3335 / iEM3350 / iEM3355 / iEM3365 / iEM3375:
  • When the meter is associated with a contactor, connect the meter upstream of the contactor.

  • The meter must be protected by a circuit breaker.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?