DOCA0005EN-15

Hardening

Recommendations to optimize cybersecurity in a protected environment:

  • Harden the device according to your company policies and standards.

  • Review assumptions about protected environments and address potential risks and mitigation strategies.

  • Least functionality can be applied to prohibit and restrict the use of unnecessary functions, protocols and/or services.

  • Change the communication protocol ports from their default values. This lowers the predictability of port use.

  • Disable communication protocol ports when they are not in use. This reduces the attack surface.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?