DOCA0005EN-15

Configuration menu for iEM3210 / iEM3215

 

A

iEM3210 / iEM3215

 

B

iEM3210

 

C

iEM3215

     

Section

Parameter

Options

Description

Wiring

Type

  • 3PH3W
  • 3PH4W
  • 1PH2W L-N
  • 1PH2W L-L
  • 1PH3W L-L-N

Select the power system type the meter is wired to.

CT

  • 3CTs on I1, I2, I3
  • 1 CT on I1
  • 2 CTs on I1, I3

Define how many current transformers (CT) are connected to the meter and which terminals they are connected to.

CT Ratio

CT Secondary

  • 1
  • 5

Select the size of the CT secondary, in Amps.

CT Primary

1 to 32767

Enter the size of the CT primary, in Amps.

Frequency

Frequency

  • 50
  • 60

Select the frequency of the electrical power system, in Hz.

Date
(iEM3210 / iEM3215)

Date

DD-MMM-YYYY

Set the current date using the specified format.

Time
(iEM3210 / iEM3215)

Time

hh:mm

Set the time using the 24-hour format.

Pulse Output
(iEM3210)

Pulse Constant
(imp/kWh)

  • 0.01
  • 0.1
  • 1
  • 10
  • 100
  • 500

Set the pulses per kWh for the pulse output.

Pulse Width
(ms)

  • 50
  • 100
  • 200
  • 300

Set the pulse width (ON time).

Multi Tariffs
(iEM3215)

Control Mode

  • Disable
  • by Digital Input
  • by Internal Clock
  • by Communication

Select the tariff control mode:

  • Disable: the Multi Tariff function is disabled.

  • by Communication: the active tariff is control by communications. See the chapter for the applicable protocol for more information.

  • by Digital Input: the digital input is associated with the Multi Tariff function. A signal to the digital input changes the active tariff.

  • by Internal Clock: the device clock controls the active tariff. If you set the Control Mode to by Internal Clock, you must also configure the schedule. Set the time when each tariff period starts, using the 24 hour clock format (00:00 to 23:59). The start time of the next tariff is the end time of the current tariff. For example, T2 start equals the end of T1.

Contrast

Contrast

1 – 9

Increase or decrease the value to increase or decrease the display contrast.

Password
(iEM3210 / iEM3215)

Password

0 – 9999

Sets the password for accessing the meter configuration screens and resets.

Reset Config

Reset Config

Settings are reset to their defaults, except for Password. Meter restarts.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?