DOCA0005EN-15

Backlight and error / alert icon

The backlight (display screen) and error / alert icon on the top right corner of the display screen indicate the meter status.

Backlight

Error / Alert icon

Description

OFF

Device not powered ON or device is OFF

ON / Dim

OFF

LCD is in power saving mode.

ON / Normal

OFF

Normal working status.

Flashing

Flashing

Alarm / diagnosis is active.

ON / Dim

Flashing

Alarm / diagnosis is active for 3 hours and LCD is in power saving mode.

ON / Normal

ON / Dim

ON

Not active alarm. Logged alarms are not acknowledged by the user.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?