DOCA0005EN-15

Supported VIFE codes for meter configuration

NOTE: E denotes the extension bit; the hex value assumes E = 0.

VIFE code

Action

Description

bin

hex

E000 0000

00

Write and replace

Replaces the old value with the new value

E000 0111

07

Clear

Resets an accumulated value to 0 (zero)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?