DOCA0005EN-15

Example: navigating the display screens

  1. Press to scroll through the main display screens; then press to move from Partial Reactive E to Tariffs to V & I.
  2. Press to access additional screens related to main screen (if available); then press to access screens for each of the available tariffs.
  3. Press to scroll through these additional screens.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?