DOCA0005EN-15

Communications LED indicator for BACnet meters

The LED indicates the status of the meter’s communications with the network.

LED state

Description

The LED is off

Communication is not active.

The LED is flashing

Communication is active.

NOTE: The LED flashes even if there is a communications error.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?