DOCA0005EN-15

Energy and energy by tariff measurements

Most energy values are available in both signed 32-bit integer and floating point format. The SNVT is appended with _l for 32-bit integer values and _f for floating point values.

For example, the SNVTs for total active energy import are as follows:

  • 32-bit integer: SNVT_elec_kwh_l

  • Floating point: SNVT_elec_whr_f

The energy and energy by tariff measurements listed below are preserved through power failures.

Network variable label

Type

Description

nvoTotkWhImp

SNVT_elec_kwh_l

Total active energy import

nvoTotkWhExp

SNVT_elec_kwh_l

Total active energy export

nvoTotkVARhImp

SNVT_elec_kwh_l

Total reactive energy import

nvoTotkVARhExp

SNVT_elec_kwh_l

Total reactive energy export

nvoTotWhImp

SNVT_elec_whr_f

Total active energy import

nvoTotWhExp

SNVT_elec_whr_f

Total active energy export

nvoTotVARhImp

SNVT_elec_whr_f

Total reactive energy import

nvoTotVARhExp

SNVT_elec_whr_f

Total reactive energy export

nvoPartialkWh

SNVT_elec_kwh_l

Partial active energy import

nvoPartialkVARh

SNVT_elec_kwh_l

Partial reactive energy import

nvoPartialWh

SNVT_elec_whr_f

Partial active energy import

nvoPartialVARh

SNVT_elec_whr_f

Partial reactive energy import

nvoPh1kWh

SNVT_elec_kwh_l

Active energy import phase 1

nvoPh2kWh

SNVT_elec_kwh_l

Active energy import phase 2

nvoPh3kWh

SNVT_elec_kwh_l

Active energy import phase 3

nvoPh1Wh

SNVT_elec_whr_f

Active energy import phase 1

nvoPh2Wh

SNVT_elec_whr_f

Active energy import phase 2

nvoPh3Wh

SNVT_elec_whr_f

Active energy import phase 3

nvoTariffActRate

SNVT_count

Active tariff:

  • 0 = Multi Tariff feature is disabled
  • 1 = rate A (tariff 1) active
  • 2 = rate B (tariff 2) active
  • 3 = rate C (tariff 3) active
  • 4 = rate D (tariff 4) active

nvoTariffAkWh

SNVT_elec_kwh_l

Rate A (tariff 1) active energy import

nvoTariffBkWh

SNVT_elec_kwh_l

Rate B (tariff 2) active energy import

nvoTariffCkWh

SNVT_elec_kwh_l

Rate C (tariff 3) active energy import

nvoTariffDkWh

SNVT_elec_kwh_l

Rate D (tariff 4) active energy import

nvoTariffAWh

SNVT_elec_whr_f

Rate A (tariff 1) active energy import

nvoTariffBWh

SNVT_elec_whr_f

Rate B (tariff 2) active energy import

nvoTariffCWh

SNVT_elec_whr_f

Rate C (tariff 3) active energy import

nvoTariffDWh

SNVT_elec_whr_f

Rate D (tariff 4) active energy import

nvoInMeterAcc

SNVT_count_f

Input metering accumulation

nvoRstEnergyDT

SNVT_time_stamp

Date and time of last energy reset

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?