DOCA0005EN-15

Device configuration

The default factory settings (as applicable based on your model) are listed in the table below:

Menu

Factory settings

Wiring

iEM3100 series: 3PH4W

iEM3200 series: 3PH4W; 3 CTs on I1, I2, and I3; Direct-No VT

iEM3300 series: 3PH4W

CT Ratio

Varies depending on meter model

CT & VT Ratio

Varies depending on meter model

Frequency

50 Hz

Date

1-Jan-2000

Time

00:00:00

Multi Tariffs

Disable

Overload Alarm

Disable

Digital Output

Disable

Digital Input

Input Status

Pulse Output

100 imp/kWh

Communication

Varies depending on protocol

Com.Protection

Enable

Contrast

5

Password

0010

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?