DOCA0005EN-15

PF lead / lag convention

The meter correlates leading power factor (PF lead) or lagging power factor (PF lag) with whether the current waveform is leading or lagging the voltage waveform.

Current phase shift from voltage

For purely resistive loads the current waveform is in phase with the voltage waveform. For capacitive loads, current leads voltage. For inductive loads, current lags voltage.

Current lead / lag and load type

Current and voltage in phase (resistive) Current leads voltage (capacitive) Current lags voltage (inductive)

Power and PF lead / lag

PF lead / lag summary

NOTE: The lagging or leading distinction does NOT equate to a positive or negative value. Rather, lagging corresponds to an inductive load, while leading corresponds to a capacitive load.

Quadrant

Current phase shift

load type

Quadrant 1

Current lags voltage

Inductive

PF lag

Quadrant 2

Current leads voltage

Capacitive

PF lead

Quadrant 3

Current lags voltage

Inductive

PF lag

Quadrant 4

Current leads voltage

Capacitive

PF lead

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?