DOCA0005EN-15

Overload alarm setup and acknowledgment

Use the information in the table below to configure the overload alarm.

NOTE: E denotes the extension bit; the hex value assumes E = 0.

SND_UD code

Data format

Manufacturer specific VIFE

Range/Options

Description

bin

hex

00

05

E011 0101

35

0 – 9999999

The pickup setpoint in kW for the overload alarm

00

02

E011 0100

34

0, 1

Overload alarm setup:

  • 0 = Disable
  • 1 = Enable

Use the information in the table below to acknowledge the overload alarm.

NOTE: E denotes the extension bit; the hex value assumes E = 1.

SND_UD code

Data format

Manufacturer specific VIFE

Range/Options

Description

bin

hex

07

00

E011 1000

B8

Acknowledge alarm

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?