DOCA0005EN-15

Configuring basic communication parameters

Before communicating with the meter using BACnet protocol, use the front panel to configure the following settings:

Setting

Possible values

Baud rate

  • 9600
  • 19200
  • 38400
  • 57600
  • 76800

Mac Address

1 – 127

Device ID

0 – 4194303

Make sure that the Mac Address is unique on the serial loop and the Device ID is unique in your BACnet network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?