DOCA0005EN-15

PF firmware updates (iEM3155 / iEM3255 / iEM3355)

Addition to PF Registers: Values ranging from +1 to -1

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

0x0C77

3192

R

2

Float32

Power Factor Total IEC

0x0C79

3194

R

2

Float32

Power Factor Total Lead Lag

0x0C7B

3196

R

1

UInt16

Power Factor Total IEC

0x0C7C

3197

R

1

UInt16

Power Factor Total Lead Lag

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?