DOCA0005EN-15

Communications setup

SND_UD code

Data format

Primary VIF

Range/Options

Description

00

01

7A

0 – 250

Primary address

To change the baud rate using communications, send a telegram to the meter with the appropriate value in the CI-field:

Baud rate

Hex value for CI-field

300

B8

600

B9

1200

BA

2400

BB

4800

BC

9600

BD

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?