DOCA0005EN-15

Data formats used by the meter (DIF bits 3 – 0)

NOTE: x in the hex value is determined by bits 7 – 4 of the DIF.

Format

bin

hex

No data

0000

x0

8-bit integer

0001

x1

16-bit integer

0010

x2

24-bit integer

0011

x3

32-bit integer

0100

x4

32-bit real

0101

x5

48-bit integer

0110

x6

64-bit integer

0111

x7

Variable length

1101

xD

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?