DOCA0005EN-15

Fixed data header

Byte 1 – 4

Identification No.

Byte 5 – 6

Manufacturer

Byte 7

Version

Byte 8

Medium

Byte 9

Access No.

Byte 8

Status

Byte 11 – 12

Signature

Serial number of the meter in an 8-digit, BCD coded format

The serial number can also be found on the meter front panel

4CA3 hex = Schneider Electric

Firmware version of the communications board

10 = version 1.0

02 hex (electricity)

Counter of successful access attempts

Indicates M-Bus application errors

Not used

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?