DOCA0005EN-15

Energy, energy by tariff and input metering

Most energy values are available in both signed 64-bit integer and 32-bit floating point format.

The energy and energy by tariff measurements listed below are preserved through power failures.

Energy reset and active tariff information

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

0x0CB3

3252

R

4

DATETIME

Energy Reset Date and Time

0x0DE1

3554

R

4

DATETIME

Input Metering Accumulation Reset Date and Time

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

0x105E

4191

R/WC

1

UInt16

Multi Tariffs Energy Active Rate:

  • 0: Multi Tariff disabled
  • 1 to 4: rate A to rate D
NOTE: You can only set the tariff using this method if the Tariff Mode is set to by Communication.
NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

Energy values – 64-bit integer

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

Total Energy (cannot be reset)

0x0C83

3204

R

4

Int64

Wh

Total Active Energy Import

0x0C87

3208

R

4

Int64

Wh

Total Active Energy Export

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

0x0C93

3220

R

4

Int64

VARh

Total Reactive Energy Import

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

0x0C97

3224

R

4

Int64

VARh

Total Reactive Energy Export

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

Partial Energy

0x0CB7

3256

R

4

Int64

Wh

Partial Active Energy Import

0x0CC7

3272

R

4

Int64

VARh

Partial Reactive Energy Import

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

Phase Energy

0x0DBD

3518

R

4

Int64

Wh

Active Energy Import Phase 1

0x0DC1

3522

R

4

Int64

Wh

Active Energy Import Phase 2

0x0DC5

3526

R

4

Int64

Wh

Active Energy Import Phase 3

Input Metering Counter

0x0DE5

3558

R

4

Int64

Unit

Input Metering Accumulation

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

Energy by Tariff (iEM3155 / iEM3255 / iEM3355 only)

0x1063

4196

R

4

Int64

Wh

Rate A Active Energy Import

0x1067

4200

R

4

Int64

Wh

Rate B Active Energy Import

0x106B

4204

R

4

Int64

Wh

Rate C Active Energy Import

0x106F

4208

R

4

Int64

Wh

Rate D Active Energy Import

Energy values – 32-bit floating point

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

Total Energy (cannot be reset)

0xB02B

45100

R

2

Float32

kWh

Total Active Energy Import

0xB02D

45102

R

2

Float32

kWh

Total Active Energy Export

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

0xB02F

45104

R

2

Float32

kVARh

Total Reactive Energy Import

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

0xB031

45106

R

2

Float32

kVARh

Total Reactive Energy Export

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

Partial Energy

0xB033

45108

R

2

Float32

kWh

Partial Active Energy Import

0xB035

45110

R

2

Float32

kVARh

Partial Reactive Energy Import

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

Phase Energy

0xB037

45112

R

2

Float32

kWh

Active Energy Import Phase 1

0xB039

45114

R

2

Float32

kWh

Active Energy Import Phase 2

0xB03B

45116

R

2

Float32

kWh

Active Energy Import Phase 3

Input Metering Counter

0xB03D

45118

R

2

Float32

Unit

Input Metering Accumulation

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

Energy by Tariff (iEM3155 / iEM3255 / iEM3355 only)

0xB03F

45120

R

2

Float32

kWh

Rate A Active Energy Import

0xB041

45122

R

2

Float32

kWh

Rate B Active Energy Import

0xB043

45124

R

2

Float32

kWh

Rate C Active Energy Import

0xB045

45126

R

2

Float32

kWh

Rate D Active Energy Import

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?