DOCA0005EN-15

Modbus communications settings

Before communicating with the device using Modbus protocol, use the display to configure the following settings:

Settings

Possible values

Baud rate

9600 Baud

19200 Baud

38400 Baud

Parity

Odd

Even

None

NOTE: Number of stop bits = 1

Address

1 – 247

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?