MID/MIR
|
Characteristic |
Value |
Meters |
|---|---|---|
|
Electromagnetic environmental class |
E2 |
iEM3110 / iEM3115 / iEM3135 / iEM3155 / iEM3165 / iEM3175 / iEM3210 / iEM3215 / iEM3235 / iEM3255 / iEM3265 / iEM3275 / iEM3310 / iEM3335 / iEM3355 / iEM3365 / iEM3375 |
|
Mechanical environmental class |
M1 |
For MID/MIR compliance, the setting must be set to 3PH4W or 1PH4W (Total energy).
The meter complies with the MID 2014/32/EU or MIR SI 2016 No 1153 when installed in cabinets rated for IP51 or better in accordance with the instructions in DOCA0038EN, available on our website. The CE and UKCA declaration documents are available from the website. Search ECDiEM3000 for CE declaration document and UKMIRiEM3000 for UKCA declaration document.