Installing and registering the LonMaker plug-in
-
Download the plug-in and XIF file for your device from www.se.com or contact your sales representative to obtain these files.
-
Make sure Echelon LonMaker is closed.
- Navigate to the location where you saved the plug-in. Extract the files if they are in a .zip file.
- Double-click setup.exe. A welcome screen appears. Click Next.
- Select the installation folder where you want to install the plug-in. Click Browse if you want to select a different location. Click Next. A confirmation screen appears.
- Click Next to begin the installation.NOTE: If LonMaker is open, a message appears instructing you to close LonMaker and restart the plug-in installation.A screen appears when the installation is complete. Click Close.
- Navigate to and select the registration entry for the plug-in you
installed (for example, Schneider Electric iEM3275 Plugin
Registration). The LNS Plugin Registration dialog box appears, indicating that registration is complete.Make sure that the plug-in appears in the list of registered plug-ins in LonMaker before you try to connect to a meter using the plug-in. If it does not appear, you may need to re-register the plug-in.Once the plug-in is installed and registered, add the meter to LonMaker. You can either read the template (.XIF) from the device during commissioning or select the EnergyMeter5A or EnergyMeter63A template when you add the device to LonMaker.