DOCA0005EN-15

Analog value object

There is one Analog Value (AV) object available on the meter, named AV00 - Command. The available commands are listed in the following table. Enter the number in the Present_Value column in the Present_Value property of the AV object to write the associated command to the meter.

Command

Present_Value entry

Object name / description

Acknowledge Overload Alarm

20001.00

Acknowledge an overload alarm.

The alarm indicator disappears from the front panel display after you acknowledge the alarm; however, this does not address the state that caused the alarm.

Reset Partial Energy Counter

2020.00

Reset partial energy accumulation to 0.

Partial Active / Reactive Energy, Energy by Tariff and Phase Energy registers are reset.

Reset Input Metering Counter

2023.00

Resets input metering accumulation to 0.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?