DOCA0005EN-15

Modifying parameters

There are two methods for modifying a parameter, depending on the type of parameter:

  • Selecting a value in a list (for example, selecting 1PH2W L-N from a list of available power systems), or

  • Modifying a numerical value, digit by digit (for example, entering a value for the date, time or VT primary).

NOTE: Before you modify any parameters, ensure that you are familiar with the HMI functionality and navigation structure of your device in configuration mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?