Overview
Modbus is an unencrypted communication protocol. RS-485 cannot transmit encrypted data using communication protocol.
WARNING |
|---|
|
Potential compromise of system availability,
integrity, and confidentiality
Unauthorized access to the network by a malicious
user could lead to the disclosure or tampering of transmitted information.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
To avoid malicious use of the sensitive information that will be transmitted through an internal network, follow the instructions:
-
Segment the network physically or logically..
-
Restrict access to the network using standard controls such as firewalls.
-
For transmitting data over an external network, encrypt protocol transmissions over all external connections using an encrypted tunnel, TLS wrapper or a similar solution.
WARNING