Overload Alarm Setup (iEM3155 / iEM3255 / iEM3355)
|
Command Number |
Action |
Size |
Type |
Unit |
Range |
Description |
|---|---|---|---|---|---|---|
|
7000 |
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
W |
1 |
UInt16 |
— |
9 |
Alarm ID |
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
0, 1 |
|
|
|
W |
2 |
Float32 |
— |
0.0 – 1e10 |
Pickup value |
|
|
W |
2 |
UInt32 |
— |
— |
(Reserved) |
|
|
W |
2 |
Float32 |
— |
— |
(Reserved) |
|
|
W |
2 |
UInt32 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
4 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
20000 |
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
W |
2 |
Float32 |
— |
— |
(Reserved) |
|
|
W |
2 |
UInt32 |
— |
— |
(Reserved) |
|
|
W |
1 |
Bitmap |
— |
0, 1 |
Digital Output to Associate:
|
|
|
20001 |
W |
1 |
UInt16 |
— |
— |
Acknowledge the Overload Alarm |