DOCA0005EN-15

Basic setup

Function profile

UCPT

Struct Members

Range / Options

Description

nciCfgWiring

UCPTWiring

SystemType

0, 1, 2, 3, 11, 13

Power system configuration:

  • 0 = 1PH2W L-N
  • 1 = 1PH2W L-L
  • 2 = 1PH3W L-L with N
  • 3 = 3PH3W
  • 11 = 3PH4W
  • 13 = 1PH4 wire multi L with N

NominFreq

50, 60

Nominal frequency in Hz

VtPrimary

0 to 1000000.0

VT primary

The minimum value for VtPrimary must be equal to or greater than the value set for VtSecondary

NOTE: Applicable only for iEM3275

VtSecondary

100, 110, 115, 120

VT secondary

NOTE: Applicable only for iEM3275

CtNum

1, 2, 3

Number of CTs

NOTE: Applicable only for iEM3275

CtPrimary

1 to 32767

CT primary

NOTE: Applicable only for iEM3275

CtSecondary

1, 5

CT secondary

NOTE: Applicable only for iEM3275

VtConnType

0, 1, 2

VT connection type:

  • 0 = Direct connection
  • 1 = 3PH3W (2VTs)
  • 2 = 3PH4W (3VTs)

NOTE: Applicable only for iEM3275

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?