DOCA0005EN-15

Communications LED indicator for M-Bus meters

The communications LED indicates the status of the communications between the meter and the network as follows:

LED state

Description

The LED is flashing

Communication with the meter has been established.

NOTE: The LED flashes even if there is a communications error.

The LED is off

There is no active communication.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?