DOCA0005EN-15

Input metering setup

Function profile

UCPT

Struct Members

Range / Options

Description

nciCfgInptMetAcc

UCPTInputMetering

PulseWeight

1 – 10000

Sets the pulse weight (1 – 10000 ms)

Setting this property also sets nciDIPulseConst (UCPTDiPulseConst) to the same value.

DigitalAssociation

0, 1

Associates the digital input with input metering:

  • 0 = Digital input is not associated with input metering
  • 1 = The digital input is associated with input metering

Setting this property to 1 also updates nciDICtrlMode (UCPTDiCtrlMode) to Input Metering.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?