DOCA0005EN-15

Energy Pulse Output Setup (iEM3155 / iEM3255 / iEM3355)

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

0x0850

2129

R/WC

1

UInt16

Millisecond

Energy Pulse Duration

0x0852

2131

R/WC

1

UInt16

Digital Output Association

  • 0 = Disable
  • 1 = DO1 enable for active energy pulse output

0x0853

2132

R/WC

2

Float32

pulse/kWh

Pulse Weight

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?