DOCA0005EN-15

Communications settings information

The following AI objects display information about the meter’s communications settings.

NOTE: You can access the meter’s communications configuration information over BACnet communications. However, you must use the front panel to configure the meter’s settings.

Object ID

Units

Default COV

Object name / description

00

1

AI00 - BACnet MAC Address

01

1

AI01 - BACnet Baud Rate

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?