DOCA0005EN-15

Overview of meter functions

The meters provide the essential measurement capabilities (for example, current, voltage, and energy) required to monitor a 1-phase or 3-phase electrical installation.

The key features of the meters are:

  • Measurement of active and reactive energy

  • Multi Tariffs (up to 4) controlled by internal clock, digital inputs or communication

  • MID/MIR compliance for many of the meters

  • Pulse outputs

  • Display (current, voltage, and energy measurements)

  • Communications via Modbus, LonWorks, M-Bus or BACnet protocols

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?