DOCA0005EN-15

Installing the M-Bus tool

Before you install the tool, you need to download it from www.se.com or obtain it from your sales representative.
  1. Navigate to the location where you saved the installation files.
  2. Double-click setup.exe. A welcome screen appears. Click Next.
  3. Confirm the installation location for the tool. Click Browse if you want to select a different location. Click Next. A confirmation screen appears.
  4. Click Next to begin the installation. A screen appears when the installation is complete.
  5. Click Close.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?