DOCA0005EN-15

Resets

Network variable label

Type

Description

Action

nciRstPartEnergy

SNVT_switch

Resets all partial energy accumulators to 0:

  • Partial active energy import (nvoPartialkWh, nvoPartialWh)
  • Partial reactive energy import (nvoPartialkVARh, nvoPartialVARh)
  • Rate A active energy import (nvoTariffAkWh, nvoTariffAWh)
  • Rate B active energy import (nvoTariffBkWh, nvoTariffBWh)
  • Rate C active energy import (nvoTariffCkWh, nvoTariffCWh)
  • Rate D active energy import (nvoTariffDkWh, nvoTariffDWh)
  • Active energy import phase 1 (nvoPh1kWh, nvoPh1Wh)
  • Active energy import phase 2 (nvoPh2kWh, nvoPh2Wh)
  • Active energy import phase 3 (nvoPh3kWh, nvoPh3Wh)

To reset, set the state field to 1.

nciRstInMeterAcc

SNVT_switch

Resets input metering accumulation (nvoInMeterAcc) to 0

To reset, set the state field to 1.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?