DOCA0005EN-15

Browsing the meter using the LonMaker plug-in

In order to use the plug-in to view data and configure the meter:
  • The plug-in must be installed and registered.

  • The meter must be added to LonMaker and commissioned.

  1. Open LonMaker.
  2. Right-click the meter icon and select Browse. The meter plug-in appears.
    NOTE: If the meter-specific plug-in does not open, the plug-in may not be correctly registered or the meter may not be properly commissioned in LonMaker. Double-check the registration and meter commissioning. Refer to the Echelon LonMaker documentation for more information.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?