DOCA0005EN-15

Digital output setup

NOTE: E denotes the extension bit; the hex value assumes E = 0.

SND_UD code

Data format

Manufacturer specific VIFE

Range/Options

Description

bin

hex

00

02

E001 1010

1A

2, 3, 0xFFFF

Digital output control mode:

  • 2 = Alarm
  • 3 = Energy (energy pulsing)
  • 0xFFFF = Disable

00

05

E010 1110

2E

iEM3135 / iEM3335:

  • 1, 10, 20, 100, 200, 1000

iEM3235:

  • 0.01, 0.1, 1, 10, 100, 500

Pulse constant

NOTE: This information only applies if the digital output control mode is set to for Pulse.

00

02

E010 1100

2C

50, 100, 200, 300

Pulse width in ms

NOTE: This information only applies if the digital output control mode is set to for Pulse.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?