LonMaker plug-in interface
The plug-in has the following tabs:
|
Tab name |
Description |
|---|---|
|
Meter Info |
This tab provides basic information about the meter (for example, model and serial number) and any active error codes. |
|
Energy Measure |
This tab provides total and partial energy values as well as energy per phase and energy by tariff information. You can also reset energy and input metering accumulations on this tab. |
|
RMS Measure |
This tab provides power, current, and voltage values as well as frequency and power factor information. |
|
Meter Status |
This tab provides information on the settings and status of the digital input and alarms as well as existing power system settings. |
|
Meter Config |
This tab provides access to the meter configuration properties, allowing you to configure power system, digital input, alarm, Multi Tariff and time settings. NOTE: If you see a message that the configuration
was unsuccessful, make sure: 1) the meter is properly commissioned
in LonMaker and the plug-in is communicating with the meter, and 2)
that Com. Protection is disabled on the meter.
|
|
Diagnostics |
This tab provides LonMaker diagnostics information related to the meter. |