DOCA0005EN-15

M-Bus protocol support

The meter supports the M-Bus protocol as follows:

  • Mode 1 communications (least significant bit first).

  • Telegram formats:

    • Single character

    • Short frame

    • Long frame

  • Function codes (C-field bits 3-0):

    • SND_NKE: Initiates of communications between the master and slave.

    • SND_UD: The master sends user data to the slave.

    • REQ_UD2: The master requests Class 2 user data from the slave.

    • RSP_UD: The slave sends requested data to the master.

  • Secondary addressing in accordance with the M-Bus standard.

  • Broadcast telegrams.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?