Primary VIFE codes used by the meter
The primary VIFE codes in the table below are used by the meter when the VIF equals FD hex (1111 1101 bin).
|
Primary VIFE codes |
bin |
hex |
Additional information |
|---|---|---|---|
|
Manufacturer |
E000 1010 |
xA |
— |
|
Model |
E000 1100 |
xC |
— |
|
Voltage |
E100 1001 |
x9 |
Volts with a resolution of 100 |
|
Current |
E101 1100 |
xC |
Amps with a resolution of 100 |
|
Digital output |
E001 1010 |
xA |
— |
|
Digital input |
E001 1011 |
xB |
— |
|
Cumulation counter |
E110 0001 |
x1 |
Input metering accumulation |
|
Error flag |
E001 0111 |
x7 |
— |