DOCA0005EN-15

BACnet protocol support

Go to www.se.com and search for your meter model to access the PICS (Protocol Implementation Conformance Statement) for your meter.

The meter supports the BACnet protocol as follows:

BACnet component

Description

Protocol version

1

Protocol revision

6

Standardized device profile (Annex L)

BACnet Application Specific Controller (B-ASC)

BACNet Interoperability Building Blocks (Annex K)

DS-RP-B (Data Sharing - Read Property - B)

DS-RPM-B (Data Sharing - Read Property Multiple - B)

DS-WP-B (Data Sharing - Write Property - B)

DS-COV-B (Data Sharing - COV - B)

DM-DDB-B (Device Management - Dynamic Device Binding - B)

DM-DOB-B (Device Management - Dynamic Object Binding - B)

DM-DCC-B (Device Management - Device Communication Control - B)

Data link layer options

MS/TP master (clause 9)

Baud rates 9600, 19200, 38400, 57600, 76800

Character set

ANSI X3.4

Supported services

  • subscribeCOV
  • readProperty
  • readPropertyMultiple
  • writeProperty
  • deviceCommunicationControl
  • who-HAS
  • who-Is
  • I-Am
  • I-Have
  • Confirmed COV notification
  • Unconfirmed COV notification

Segmentation

The meter does not support segmentation

Static device address binding

The meter does not support static device address binding

Networking options

None

The following standard object types are supported:

Object type

Optional properties supported

Writeable properties supported

Proprietary properties

Device Object

  • Max_Master
  • Max_Info_Frames
  • Description
  • Location
  • Local_Date
  • Local_Time
  • Active_COV_Subscriptions
  • Profile Name
  • Object_Name
  • Max_Master
  • Max_Info_Frames
  • Description
  • Location
  • APDU_Timeout
  • Number_Of_APDU_Retries

D_800

ID_801

ID_802

Analog Input Object

COV_Increment

Analog Value Object

Binary Input Object

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?