DOCA0005EN-15

Power system wiring: iEM3100 / iEM3300 series

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not connect N’ to the load when setting the wiring type on the meter to 1PH4W Multi L-N.
Failure to follow these instructions will result in death or serious injury.

1PH2W LN≤ 240 V L-N

1PH2W LL≤ 415 V L-L

1PH3W LLN≤ 240 V L-N
≤ 480 V L-L

1PH multiple load with N

3PH3W≤ 480 V L-L

3PH4W≤ 240 V L-N
≤ 480 V L-L

Fuses and disconnect switch

Clearly label the device’s disconnect circuit mechanism and install it within easy reach of the operator.

Fuses / circuit breakers must be:

  • Installed in accordance with all local and national electrical codes and standards.

  • Rated for the installation voltage, available fault current, and sized for connected loads.

Fuse for neutral is required if the source neutral is not grounded.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?