DOCA0005EN-15

Communications LED indicator for Modbus devices

The yellow communications LED indicates the status of communication between the meter and the master as follows:

If...

Then...

The LED is flashing

Communication with the device has been established.

NOTE: If there is an error online, the LED also flashes.

The LED is off

There is no active communication between the master and the slave

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?